AnsweredAssumed Answered

Kinetis K60 Microcontroller for Motor Control Application

Question asked by Kannan A on Jun 20, 2014
Latest reply on Jun 20, 2014 by Perla Andrea Moncada Fajardo

Hi,

 

We referred one of your application note( AN Name: BLDC Motor Control for Respirators), Which states that Kinetis K60 is capable of controlling BLDC motor up to 60,000 RPM.

 

We need Micro controller, Which is capable of controlling BLDC motor up to 60,000 RPM for Medical Respirator device.

 

Please share more details of above microcontroller for BLDC motor control application.

 

We wanted to understand what will be the percentage of CPU utilization if the motor is run at full 60000RPM. Will this controller be good for his application or whether he should consider some other option for the same.

 

Please suggest.

 

 

Thanks,

Kannan

Outcomes