Hi..
I am currently using iMX536 AI rev B board for my project. I want to know whether I can implement TTCAN (Time Triggered
CAN) in the same board and how ?
Hi Sandeep
in general yes, because
TTCAN is a higher-layer protocol above the
unchanged standard CAN protocol that synchronises
the communication schedules of
all CAN nodes in a network and that provides
a global system time.
Regarding how, I think you should look at CAN
related linux sources, ISO11898-1, since this is very specific subject.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Chipexpert,
I already checked the ISO11898-1 standard. But the problem is there are no tips for the implementation. They only explain what is TTCAN. Do anyone in this community possess any source code for TTCAN ? If yes please share.
Hi Sandeep
unfortunately i.MX Freescale BSPs do not have these codes.
Best regards
chip
Hi igorpadykov,
I am also trying to implementing the TTCAN based communication on my MPC 5777M. I have gone through the RM , but I am little bit confused to implement. Is there any sample code for TT _CAN for same or similar mpc 5xxx?@igorpadykov@martin kovar,petr stancik