AnsweredAssumed Answered

How to remove PMIC driver from freescale BSP in Yocto Project

Question asked by arun kumar on Jun 18, 2014
Latest reply on Jun 18, 2014 by igorpadykov

Hi, i have build the freescale BSP using the Yocto project and running the image on iMX6SL EVK. What i want to do next is remove the PMIC driver. I have created a different EVK board with differ PMIC than what is being used on the Freescale EVK. Any pointers on how i can remove the PMIC driver functionality from the BSP and build the image so it can run on the board that i have made with different PMIC. On my board all the voltage rails will come up as default so no interaction is needed from the SOC.

 

Regards,

Arun

Outcomes