Hi,
I'm trying to use bean IntEEProm for MC9S08PA16 but when I put the address 0x3100 as a start adrress of EEProm the CodeWarrior gives me a error "Memory is already used for the component CPU".
What's the problem?
This is my first time I'm using internal EEPROM to write data.
If there is a better way to do the same, please send me.
Thanks a lot
Edson
Hi Edson,
Sorry for the delay.
By default when you create a project through the wizard for S08PA16 with Processor Expert (PE), PE will generate the linker parameter file (.prm).
The EEPROM module is already defined for the prm:
After to added the Bean
Component: IEE1 of type IntEEPROM
Description: Internal EEPROM
You must modify the Memory mapping.
So I've disable the Memory Area4.
Now the error disappears and I can generate PE code and build the project without problem.
Attached you will find the project used ...
Hope this will help you.
Have a great day,
Pascal
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------