AnsweredAssumed Answered

enable DISP0

Question asked by Raphael Spies on Jun 18, 2014
Latest reply on Jun 30, 2014 by Raphael Spies

Hello,

 

At the moment I started working with the iMX6. We built our own Board for the iMX6 and now are trying to figure out how to get the display output to the DISP0 pins.

The output worked fine on a phyflex carrier board for the hdmi and the lvds output but now we have to use the lcd output.

 

I have installed the image from phytec on the board (ftp://ftp.phytec.com/products/PFL-A-02_phyFLEX-iMX6/Linux/PD13.2.3/BSP-Phytec-phyFLEX-i.MX6-PD13.2.3.tar.gz) but cannot figure out how to change the video output to the lcd.

 

In the quickstart from phytec it is written how to change between LVDS and HDMI ( PhyFLEX-i.MX6 Linux Quickstart-PD13.2.0 - PHYTEC Wiki ) but no comment about the lcd. Also the command (edit env/display/bootargs-display) to change the bootargs is not working because the requested file with the lines to edit is not existing.

I wanted to set the bootargs-display to something like:

 

video=mxcfb0:dev=lcd,800x480,if=RGB624


but could not figure out how to set the bootargs properly.

 

Can anyone help me?

 

 

Thanks a lot!

Outcomes