Cristopher Lubay

HCS08 Timer Value (minimum)

Discussion created by Cristopher Lubay on Aug 30, 2007
Latest reply on Aug 30, 2007 by David Payne
I'm currently using an HCS08AW32 microcontroller.
I would like to make a PWM using 1 of the channels of the microcontroller timer.
I can use the timer channel but if I set the timer to a value of less than 50 microseconds, the debugger resets.
What is the minimum value that can be used for the timer channels?
Can I use the timer to as low as 5 microseconds?
Is there a special setting in order for me to be able to use it to as low as 5 us?
Thank you!

Outcomes