AnsweredAssumed Answered

bitbake fsl-image-core failure for T1040rdb

Question asked by Chandra Shekhar on Jun 13, 2014
Latest reply on Nov 12, 2017 by Erik Raynolds

Hi all,

 

I am not able to build "bitbake fsl-image-core" for t1042rdb board on Ubuntu 14.04. Below is the log message,

 

---------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

asr907@asr907-ThinkStation-S20:~/sdk/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1042rdb_release$ bitbake fsl-image-core

Pseudo is not present but is required, building this first before the main build

WARNING: Host distribution "Ubuntu-14.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.

Loading cache: 100% |########################################################################################################################################################################| ETA:  00:00:00

Loaded 3156 entries from dependency cache.

 

Build Configuration:

BB_VERSION        = "1.18.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-14.04"

TARGET_SYS        = "powerpc-fsl-linux"

MACHINE           = "t1042rdb"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "1.4.1"

TUNE_FEATURES     = "m32 fpu-hard e5500"

TARGET_FPU        = "hard"

meta             

meta-yocto       

meta-yocto-bsp    = "(detachedfromb96dbe8):b96dbe8f38042e0b88b93e2d6385a891fbd34c6c"

meta-fsl-ppc      = "(detachedfromfcfbc80):fcfbc80d54646f3a414e597a04215c00c3a30fc8"

meta-fsl-ppc-toolchain = "(detachedfroma01e15a):a01e15a765c6082c5e2236c05eca9469859d0725"

meta-fsl-networking = "(detachedfroma27ce2f):717d73da6548d7b27acb659f6f15f4cd7b4af062"

meta-virtualization = "(detachedfrom0c26da8):0c26da86404a5421f579188d24864aea05c9611a"

meta-oe          

meta-networking   = "(detachedfrom8c5e175):8c5e175603b0163d57e94216088b9acc203f3a73"

 

NOTE: Resolving any missing task queue dependencies

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Function failed: sysroot_stage_all (see /home/asr907/sdk/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1042rdb_release/tmp/work/x86_64-linux/quilt-native/0.60-r0/temp/log.do_populate_sysroot.5463 for further information)

ERROR: Logfile of failure stored in: /home/asr907/sdk/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1042rdb_release/tmp/work/x86_64-linux/quilt-native/0.60-r0/temp/log.do_populate_sysroot.5463

Log data follows:

| DEBUG: Executing python function sstate_task_prefunc

| DEBUG: Python function sstate_task_prefunc finished

| DEBUG: Executing python function do_populate_sysroot

| DEBUG: Executing shell function sysroot_stage_all

| tar: --same-order option cannot be used with -c

| Try 'tar --help' or 'tar --usage' for more information.

| tar: This does not look like a tar archive

| tar: Exiting with failure status due to previous errors

| DEBUG: Python function do_populate_sysroot finished

| ERROR: Function failed: sysroot_stage_all (see /home/asr907/sdk/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1042rdb_release/tmp/work/x86_64-linux/quilt-native/0.60-r0/temp/log.do_populate_sysroot.5463 for further information)

ERROR: Task 10 (/home/asr907/sdk/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/meta/recipes-devtools/quilt/quilt-native_0.60.bb, do_populate_sysroot) failed with exit code '1'

NOTE: Tasks Summary: Attempted 23 tasks of which 22 didn't need to be rerun and 1 failed.

No currently running tasks (7 of 63)

 

Summary: 1 task failed:

  /home/asr907/sdk/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/meta/recipes-devtools/quilt/quilt-native_0.60.bb, do_populate_sysroot

Summary: There was 1 WARNING message shown.

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

asr907@asr907-ThinkStation-S20:~/sdk/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1042rdb_release$

---------------------------------------------------------------------------------------------------------------------------------------------

 

Can someone suggest what is missing here?

 

Regards,

-Chandra

Outcomes