AnsweredAssumed Answered

USB Enumeration Pass through

Question asked by SIVA KUMAR on Jun 10, 2014
Latest reply on Jun 13, 2014 by jeremyzhou

Hello Team,

 

We are working on a project please guide us is our requirement is achievable or not.

 

We would like to use k70 in our project. The K70 has USB interface can be acted as host and gadget.

Is the enumeration of the host can be passed to gadget driver dynamically? 

 

For better understanding see the following example.

 

The K70 is connected to PC as a gadget and any USB device(3G/Wi-Fi dongle) is connected to the K70 then the

enumeration from the K70 host should be passed to gadget driver dynamically.

The PC should see the USB device(3G/Wi-Fi dongle) is it possible.

 

If it can be done how complex in making it work?

 

Thanks & Regards,

Siva Kumar

Outcomes