We are currently trying to bring up the DPAA interfaces on T4240QDS. We are trying to use the on-board ETH PHY MACs for enabling the DPAA (These are on RGMII)
We are using Yocto SDK 1.4 version and have followed the documentation in SDK to configure USDPAA
root@t4240qds:/usr/etc# fmc -c usdpaa_config_t4_serdes_1_1_6_6.xml usdpaa_policy_hash_ipv4.xml -a
ERR : Invocation of FM_PORT_Open for fm1/port/10G/0 failed
ERR : Invocation of FM_PCD_Disable for fm0/pcd failed with error code 0x00010028
Also while using uImage-t4240qds-usdpaa.dtb Ethernet links FM1-MAC5 and FM3-MAC5 are not getting detected. Only lo,sit0,tunl0 are present whereas in uImage-t4240qds.dtb we are able to set ip and also ping other sytems for fm1-mac5 and fm3-mac5.
Our uboot environment variables are
baudrate=115200
bdev=sda3
bootargs=root=/dev/mmcblk0p1 rw rootdelay=5 console=ttyS0,115200 usdpaa_mem=256M bportals=s0-1 qportals=s0-1
bootcmd=setenv bootargs root=/dev/mmcblk0p1 rw rootdelay=2 console=$consoledev,$baudrate;mmcinfo;ext2load mmc 0:1 $loadaddr $bootfile;ext2load mmc 0:1 $fdtaddr $fdtfile; bootm $loadaddr - $fdtaddr
bootdelay=3
bootfile=uImage
consoledev=ttyS0
eth10addr=00:04:9F:02:7A:39
eth11addr=00:04:9F:02:7A:3A
eth12addr=00:04:9F:02:7A:3B
eth13addr=00:04:9F:02:7A:3C
eth14addr=00:04:9F:02:7A:3D
eth15addr=00:04:9F:02:7A:3E
eth1addr=00:04:9F:02:7A:30
eth2addr=00:04:9F:02:7A:31
eth3addr=00:04:9F:02:7A:32
eth4addr=00:04:9F:02:7A:33
eth5addr=00:04:9F:02:7A:34
eth6addr=00:04:9F:02:7A:35
eth7addr=00:04:9F:02:7A:36
eth8addr=00:04:9F:02:7A:37
eth9addr=00:04:9F:02:7A:38
ethact=FM1@DTSEC5
ethaddr=00:04:9F:02:7A:2F
ethprime=FM1@DTSEC5
fdtaddr=0x17200000
fdtfile=uImage-t4240qds.dtb
fileaddr=1000000
filesize=46573C
fman_ucode=0xeff40000
gatewayip=192.168.1.1
hwconfig=fsl_ddr:ctlr_intlv=3way_4KB,bank_intlv=auto;fsl_fm1_xaui_phy:xfi;fsl_fm2_xaui_phy:xfi
ipaddr=10.116.65.141
loadaddr=0x10000000
netdev=eth0
netmask=255.255.255.0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr
ramdiskaddr=2000000
ramdiskfile=t4240qds/ramdisk.uboot
rcw=t4240rcw
rcw_spi=mw.w ffdf0060 2201;qixis_reset altbank
rcwemmc=mw.w ffdf0060 2000
rootpath=/opt/nfsroot
sataboot=setenv bootargs root=/dev/sda1 rootdelay=5 rw console=$consoledev,$baudrate $othbootargs;bootm e8020000 - e8800000
sdboot=setenv bootargs root=/dev/mmcblk0p1 rw rootdelay=5 console=ttyS0,115200; ext2load mmc 0:1 $loadaddr $bootfile; ext2load mmc 0:1 $fdtaddr $fdtfilel bootm $loadaddr - $fdtaddr
serverip=10.116.65.150
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddr +$filesize && cmp.b $loadaddr $ubootaddr $filesize
tftprcw=tftpboot $loadaddr $rcw && mmcinfo && mmc write 1000000 8 1
uboot="u-boot.bin"
ubootaddr=0xeff80000
We have also attached the current RCW source file and the DTS file (that we are using to build the image) as well as the boot log file.
Kindly let us know the changes that we have to make to get this working.
Thanks,
Amit
Original Attachment has been moved to: bootlog.zip
Original Attachment has been moved to: rcw_1_1_6_6_1666MHz.rcw.zip
Original Attachment has been moved to: t4240qds-usdpaa.dts.zip
Please check the following whether you missed something.
On the target board
$ cd /usr/etc
$ fmc -c {Serdes Config File} -p {Policy File} -a
$ reflector -c {Serdes Config File} -p {Policy File}
You will launch reflector and enter reflector prompt.
reflector> help
reflector> add 0..{ Num of cores - 1 }
On the Linux host side, add ARP records
arp -s { target IP } { Port Mac Addr }
Then Ping { IP }
If you problem remains, please kindly share your Linux console log.
Have a great day,
Yiping Wang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------