AnsweredAssumed Answered

About the minimum clock frequency of the core for i.MX6 Solo

Question asked by yuuki on Jun 4, 2014
Latest reply on Jun 5, 2014 by Anson Huang

Dear all,

 

Would you teach about the minimum clock frequency of the core for i.MX6 Solo?

 

According to the "Table 9. Operating Ranges" of a datasheet, the following is indicated.
- Run mode: LDO enabled => VDD_ARM_IN : 1.175-1.5V "LDO Output Set Point (VDD_ARM_CAP) = 1.05 V minimum for operation up to 396 MHz."
- Run mode: LDO bypassed => VDD_ARM_IN : 1.05-1.3V "LDO bypassed for operation up to 396 MHz"

 

However, the minimum is not shown.

 

Would you teach the minimum CPU Core clock frequency in which the system can operate?

 

Best Regards,

Outcomes