Hi,
We got a reference board T1040-QDS-D3 - QorIQ Development System. But we are not able to boot it. We are not getting console messages. We have probed NOR flash control signals (CE#, WE#, OE#) on test points TP161, TP162, TP163. These are coming properly. So can anyone please tell how we can get console??
I am not sure whether there is valid images on your target.
Please refer to the following default switch setting for T1040QDS.
SW1 : 0x13 = 00010011 SW5 : 0xef = 11101111 SW9 : 0xa0 = 10100000
SW2 : 0xff = 11111111 SW6 : 0x0f = 00001111 SW10 : 0xea = 11101010
SW3 : 0x23 = 00100011 SW7 : 0x66 = 01100110 SW11 : 0x24 = 00100100
SW4 : 0x00 = 00000000 SW8 : 0x6c = 01101100 SW12 : 0xff = 11111111
Where '1' = up/ON
If there is no valid RCW on your target, you could use CodeWarrior 10.3.3 to flash RCW on NOR Flash.
In CodeWarrior, the NOR flash address range is from 0xE8000000 to 0xEFFFFFFF, RCW is located at
address 0xe8000000, and u-boot is at 0xeff80000.
I think you could get u-boot and RCW images from software package, if you cannot get them, you could generate RCW with QCS and build u-boot from u-boot git tree source.
Have a great day,
Yiping Wang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------