Sai Maddikayala

ELF is not in expected HALT mode (CDS8548, CW8.7, IDE5.9)

Discussion created by Sai Maddikayala on Aug 28, 2007
Latest reply on Aug 30, 2007 by Sai Maddikayala
When I try to step into next instruction or  somtimes put a break point or do a hard reset from the CodeWarrior IDE I get a message that says:

ELF is not in expected HALT mode or
ELF is not in expected STOP mode

Any idea what this means. Thanks for any inputs.

I'm using USB TAP to connect to target, with a default clock speed of 4.03 MHz.
-Sai

Outcomes