AnsweredAssumed Answered

LTIB instalation failed

Question asked by David Martinez on May 30, 2014
Latest reply on Oct 1, 2014 by Andrey Demidov

hi.

 

after run ./ltib this is the message  I read in the host_config.log. can anybory help me with this?

 

 

thanks !

 

------------------------------------------------------------------

 

Processing platform: Host support packages

============================================

using /home/david/ltib/config/platform/host/ltib.preconfig

 

 

Processing: fake-provides

===========================

 

 

Processing: mkspooflinks

==========================

 

 

Processing: distcc

====================

 

 

Processing: ccache

====================

 

 

Processing: bison

===================

 

 

Processing: flex

==================

 

 

Processing: texinfo

=====================

 

 

Processing: autoconf

======================

 

 

Processing: libtool

=====================

 

 

Processing: lkc

=================

 

 

Processing: patch

===================

 

 

Processing: wget-ssl

======================

Build path taken because: directory build, no prebuilt rpm,

 

 

Cowardly refusing to clobber existing directory:

/opt/ltib/usr/src/rpm/BUILD/wget-1.14

Remove this by hand if you really want to rebuild this package from scratch

 

 

Died at ./ltib line 1492.

traceback:

main::build_host_rpms:1492

  main::host_checks:1554

   main:562

Outcomes