Hello,
I am using custom hardware is based on i.MX535 Sabre platform
1. Bluetooth is connected to UART3 and communicate with chip based on BCSP protocol .
2. Scanning is ok.
3. File transfer , and BT audio over SCO also ok.
BUT, some times while file transferring or in BT voice call time i am getting error
bcsp_pkt_cull: Peer acked invalid packet
bcsp_handle_le_pkt: Found a LE sync pkt, card has reset
please advice how to resolve this issue .
Regards,
suman.
Hi Rajput
seems this is well know bug in BT stack, please refer to links below
How to run up CSR chip without eeprom with BLUEZ ? -- Bluez Devel
bluez - bluetooth stack for Linux - users
Probably more updated BT driver on newer kernel will help
i.MX53 Quick Start - Linux on ARM - eewiki
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------