Hi all,
I am working on Kinetis KL46 processor with SPI Flash.
I am in need of implemented SPI Flash drivers for this.
Will anyone can provide me please?
Thanking you,
Hi
The KL46 is supported in the uTasker project (TWR-KL46 and FRDM-KL46 as immediate target builds) with utFAT on SD cards via the SPI (or uFileSystem in ATMEL 45DB xxx, SST25xxx or ST 25Pxxx serial flash). See below simulations of the two boards operating with SD card and driving SLCDs.
Regards
Mark
http://www.utasker.com/kinetis.html
Hi,
In the KL46 source code you can find an example which uses the SPI module with the DMA feature. There you can find drivers for the SPI module
KL46 Source Code:
FRDM-KL46Z: Freescale Freedom Development Platform for Kinetis KL3x and KL4x MCUs
If you do not want to download the complete package in the attachments you can find the source code of this project.
Hope this helps,
Regards,
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. It would be nice!
-----------------------------------------------------------------------------------------------------------------------
Is it possible to implement the file system in SPI Flash?