Hello,
I tried compiling Ltib BSP for IMX 28 its compiling smoothly with kernel version 2.6.35..When i tried to change the kernel version to 3.0.35 am getting this error how can i solve this
Processing: kernel-3.0.35
===========================
Build path taken because: force set, no prebuilt rpm,
Testing network connectivity
OK PPP:
OK GPP:
Try linux-3.0.35.tar.bz2 from the PPP
12:56:53 URL:http://auslxsc01.am.freescale.net/ppp/linux-3.0.35.tar.bz2 [1030] -> "linux-3.0.35.tar.bz2" [1]
ERROR: md5sum mismatch, re-naming /opt/freescale/pkgs/linux-3.0.35.tar.bz2 to /opt/freescale/pkgs/linux-3.0.35.tar.bz2.bad, please re-try
Can't get: linux-3.0.35.tar.bz2 at ./ltib line 802.
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Wed May 21 12:55:27 2014
Ended: Wed May 21 12:56:53 2014
Elapsed: 86 seconds
These packages failed to build:
kernel-3.0.35
Build Failed
Exiting on error or interrupt
FSL kernel 3.0.35 does not support mx28.
If you want to try a newer kernel on mx28, just use the most recent one from kernel.org.
The Official Freescale BSP only supports Linux Kernel 2.6.35, so you need tou se Yocto BSP in order to compile the 3.0.35 BSP. You can get the details on
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------