I have written sample code for connecting mcf522559 with PC i.e Mcf52259--> PC .
I have written server code to create ppp connection
with following set parameter
ipcp_data.IP_UP = PPP_linkup;
ipcp_data.IP_DOWN = NULL;
ipcp_data.IP_PARAM = (pointer)&ppp_sem;
ipcp_data.ACCEPT_LOCAL_ADDR = TRUE;
ipcp_data.LOCAL_ADDR = PPP_LOCADDR;
ipcp_data.ACCEPT_REMOTE_ADDR = TRUE;
ipcp_data.REMOTE_ADDR = PPP_PEERADDR;
ipcp_data.DEFAULT_NETMASK = TRUE;
ipcp_data.NETMASK = 0;
ipcp_data.DEFAULT_ROUTE = TRUE;
ipcp_data.NEG_LOCAL_DNS = FALSE;
ipcp_data.ACCEPT_LOCAL_DNS = 0;
ipcp_data.LOCAL_DNS = 0;
ipcp_data.NEG_REMOTE_DNS = FALSE;
ipcp_data.ACCEPT_REMOTE_DNS = 0;
ipcp_data.REMOTE_DNS = 0;
I have also created PPP modem in PC side .I am using windows XP
But unable to connect .
Can any one tell me steps to create ppp connection in pc side .
Thanks in Advance
NIsha
Solved! Go to Solution.
Hi,
You can find the documentation and the example of how to use PPP in MQX in the next folder:
<Freescale MQX X.X>\rtcs\examples\shell
Have a great day,
Regards
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
You can find the documentation and the example of how to use PPP in MQX in the next folder:
<Freescale MQX X.X>\rtcs\examples\shell
Have a great day,
Regards
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sol,
Thanks for your reply using the shell folder only i wrote mqx code for ppp in MCF52259.
I want to set ppp connection between mcf and pc (MCF52259 -------------> PC).
I want steps to connect mcf with ppp modem in pc, I want the steps to create ppp in pc that will enable mcf through ppp to communicate with PC .
Regards,
NIsha
I got the steps to create ppp connection in pC .
It is working Fine.
Now., I want to connect MCF with Modem(PPP dial connection).
I activated ppp connection in modem using at commands and tried to connect with modem .But unable to do so.
Do i need to make any changes in the code to connect with modem ppp dial up connection.
Thanks in advance
Nisha