Luigi Mantellini

uClinux on 547x (m5475evb test board)

Discussion created by Luigi Mantellini on Aug 27, 2007
Latest reply on Aug 27, 2007 by Kenneth Wong
Hi,

I have some (stupid) questions about uclinux and the m5475evb.

1) Is this board supported by uClinux? (I found the m5475evb target... by the created image doesn't start)
2) Can I use the gcc-4.1.0-based tool-chain proposed on http://www.uclinux.org/pub/uClinux/m68k-elf-tools/?

To create the linux image, I inserted the following commands sequence:
Code:
cd ucLinux-distmake xconfig # Selecting just the M5475evb targetmake # create the image.bin in tftpboot directory

(I selected kernel 2.6.0 w/ uclibc)

 on the dBoot shell:
Code:
dBUG> dnDownloading Image 'image.bin' from 192.168.50.132TFTP transfer completed Read 2128900 bytes (4159 blocks)dBUG> go 0x20000

After the "go 0x20000" command the board seems frozen...

Can you help me? This is my first experience with coldfire/uclinux systems (and embedded systems in general).

Thanks,

luigi
 





Message Edited by comio on 2007-08-27 12:03 PM

Outcomes