hi everybody,
I have a system that works with the i.MX28 (home health hub plaform), and I need some documentation or a start guide to work with it, the platform has pre-installed linux BSP. I need some examples about how to programming and develop new projects.
can anybody help me ?
regards.
The Linux and Windows EC7 board support packages (source code included, which might help) are available for download from the Digi web site and include some demo applications.
The following slides may be of help as reference on how to set-up the demos although these do not cover how to develop new applications for the Home Health Hub Reference Platform.
to programming the HHH is necesary an aditional software or can be programmed using a serial terminal connect directly to the platform trougth usb cable.
so that I can enter to de linux OS but the commands ussually used appear like no find (for intance, sudo, apt-get).
is there any guide to start programming the HHH step by step?
regards