AnsweredAssumed Answered

MQX serialization

Question asked by Oscar Garcia Abad on May 13, 2014
Latest reply on May 13, 2014 by Oscar Garcia Abad

Hello all,

 

I'm working with a MK60FN1M0VLQ12 microcontroller. I'm running MQX 4.1 in a custom board. I'm using

codewarrior 10.5.

 

I want to put a serial code in flash at an absolute address. I will do so with cyclone MAX. I know how to make the cyclone part.

But when I wanted to define my serial code in my code I found that the gcc doesn't support the following code:

 

char Serial[SERIAL_LENGTH]@Address;

 

I found that with gcc this is made as you can see in the following link:

 

Defining Variables at Absolute Addresses with gcc | MCU on Eclipse

 

But my problem comes when I want to locate the MQX linker script.

 

Where can I find it?

 

Thanks in advance.

 

Oscar.

Outcomes