Dear community,
I have a question about internal pull-up/down resistor in i.MX6DL.
[Question]
During Reset ( power up sequence ) , is the internal pull-up/down resistor available ?
[Background]
I consider an unused pin treatment.
If the internal resistor is available during Reset,
I keep the unused pin to leave no-connect for cost saving.
Best Regards,
Koichi Sakagami
Solved! Go to Solution.
You can see which Pads has the pullup or pull down resistor enable in the Reference Manual Table 4-1. Do you have any particular pad whith a problem?
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
You can see which Pads has the pullup or pull down resistor enable in the Reference Manual Table 4-1. Do you have any particular pad whith a problem?
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Jaime san,
Thank you for your reply.
I got it .
I have no problem.
Best Regards,
Koichi Sakagami