Can't read from SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't read from SD card

Jump to solution
1,097 Views
till_klocke
Contributor I

Hello,

currently I'm trying to get the mainline linux kerne 3.12.17 working in a i-mx6 based board from Phytec. I am using the default kernel configuration for this processor and the kernel does boot via barebox from a SD card. But as soon as the kernel itself tries to access the SD card I get the following error:

mmcblk0: error -84 transferring data, sector 18692, nr 4, cmd response 0x900, card status 0x0

I can rule out a defect SD card or a problem on the board, since this happens with all SD cards I am trying, also barebox can read just fine from the SD card. The default Linux distribution (with an outdated 3.0.35 kernel) can also read fine from the SD.

I hope that someone here has an idea how I can solve this problem.

Thanks in advance.

Labels (2)
Tags (2)
0 Kudos
1 Solution
656 Views
fabio_estevam
NXP Employee
NXP Employee

I would suggest you to try 3.14.3 and if the problem still occurs, then post to linux-arm-kernel list.

View solution in original post

0 Kudos
2 Replies
657 Views
fabio_estevam
NXP Employee
NXP Employee

I would suggest you to try 3.14.3 and if the problem still occurs, then post to linux-arm-kernel list.

0 Kudos
656 Views
till_klocke
Contributor I

Thanks I tried Kernel 3.14.3 it boot just fine. So probably there is a bug in 3.12.17.

0 Kudos