Hi There,
I followed the GStreamer RTP Streaming instructions, but my system doesn't have the gstrtpbin element that is being used. However, I do have udpsrc and various other elements from the plugins-good package. When I rebuild the plugin registry I see a few errors that could be a hint to someone, but unfortunately not to me. Does anyone know what could be the problem ? I'm using the 4.1.0 BSP.
MAX resolution 800x480
(gst-plugin-scanner:3559): GLib-GObject-WARNING **: cannot register existing type `GstRtpSsrcDemux'
(gst-plugin-scanner:3559): GLib-CRITICAL **: g_once_init_leave: assertion `initialization_value != 0' failed
(gst-plugin-scanner:3559): GStreamer-CRITICAL **: gst_element_register: assertion `g_type_is_a (type, GST_TYPE_ELEMENT)' failed
(gst-plugin-scanner:3559): GStreamer-CRITICAL **: gst_pad_template_new: assertion `caps != NULL' failed
(gst-plugin-scanner:3559): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed
(gst-plugin-scanner:3559): GStreamer-CRITICAL **: gst_pad_template_new: assertion `caps != NULL' failed
(gst-plugin-scanner:3559): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion `GST_IS_PAD_TEMPLATE (templ)' failed
(gst-plugin-scanner:3559): GLib-GObject-WARNING **: cannot register existing type `GstRTPMux'
(gst-plugin-scanner:3559): GLib-CRITICAL **: g_once_init_leave: assertion `initialization_value != 0' failed
(gst-plugin-scanner:3559): GStreamer-CRITICAL **: gst_element_register: assertion `g_type_is_a (type, GST_TYPE_ELEMENT)' failed
Thanks,
/Otto
Solved! Go to Solution.
I disabled all other plugins (bad, ugly, farsight) and now the gstrtpbin showed up properly. So there has to be some form of conflict
Btw, just to clarify - I'm running this on the imx6 board. Also, here is the ./configure output during build. It looks good assuming GstRtpBin is part of the rtpmanager.
configure: *** Plug-ins without external dependencies that will be built:
alpha
apetag
audiofx
audioparsers
auparse
autodetect
avi
cutter
debugutils
deinterlace
effectv
equalizer
flv
flx
goom
goom2k1
icydemux
id3demux
imagefreeze
interleave
isomp4
law
level
matroska
multifile
multipart
replaygain
rtp
rtpmanager
rtsp
shapewipe
smpte
spectrum
udp
videobox
videocrop
videofilter
videomixer
wavenc
wavparse
y4m
configure: *** Plug-ins without external dependencies that will NOT be built:
monoscope
configure: *** Plug-ins with dependencies that will be built:
annodex
cairooverlay
oss4
ossaudio
v4l2src
configure: *** Plug-ins with dependencies that will NOT be built:
1394
aasink
cacasink
cairo
directsoundsink
dv
esdsink
flac
gconfelements
gdkpixbuf
halelements
jack
jpeg
osxaudio
osxvideosink
png
pulseaudio
shout2
souphttpsrc
speex
sunaudio
taglib
wavpack
ximagesrc
I disabled all other plugins (bad, ugly, farsight) and now the gstrtpbin showed up properly. So there has to be some form of conflict
Otto, when the conflict occurred, how did you add the elements? Did you use Yocto or LTIB to do the latter?
Leo
Leo, we are using LTIB. I'm suspecting the farsight plugins, since they also provide RTP functionality, but have not verified it yet.