Not working:ddcopy.exe for copying bootloader image to sd card on windows 8.1 64-bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not working:ddcopy.exe for copying bootloader image to sd card on windows 8.1 64-bit

840 Views
manjug
Contributor III

ddcopy.exe for copying bootloader image to sd-card is not working properly on windows 8.1 64-bit machine .It shows success status but when sd-card inserted and powered not booting.Same i tried on windows 7 it is working fine.Please help me for windows 8.1 64-bit machine.

0 Kudos
2 Replies

639 Views
soledad
NXP Employee
NXP Employee

hi,

Are you using a Freescale board??


Have a great day,
Regards
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

639 Views
manjug
Contributor III

Hello,

Yes I'm using Freescale TWR-VF65GS10 Board

0 Kudos