Hi
I am trying to install the ltib for imx53 on Fedora20
I have downloaded the L2.6.35_11.09.01_ER_source_bundle.tar.gz file,
and use the ./ltib to install that what got:
........
+ make DESTDIR=/home/PF/work/L2.6.35_11.09.01_ER/ltib/tmp/sparse PREFIX=/opt/freescale/rootfs/i686//opt/freescale/ltib/usr 'CFLAGS=-O2 -march=i686'
CC test-lexing.o
CC target.o
CC parse.o
In file included from parse.c:25:0:
parse.h:63:22: error: duplicate member 'label_statement'
struct statement *label_statement;
^
make: *** [parse.o] Error 1
error: Bad exit status from /home/PF/work/L2.6.35_11.09.01_ER/ltib/tmp/rpm-tmp.64523 (%build)
RPM build errors:
Bad exit status from /home/PF/work/L2.6.35_11.09.01_ER/ltib/tmp/rpm-tmp.64523 (%build)
Build time for sparse: 0 seconds
Failed building sparse
Died at ./ltib line 1380.
traceback:
main::build_host_rpms:1380
main::host_checks:1435
main:542
please help me to fix the problem
Thanks
PF
hi,
It is a best choice to install LTIB on Ubuntu 12.04 and most of us have successfully installed on it. Also, you can try to make image by Yacto for you IMX53 board.
regards,
Tony
any suggestions are welcome......
Thanks
PF
Hi PF,
I just have installed ltib succeed in Ubuntu. So about Fedora I just can give you some advices. Have you installed the packages needed by LTIB? And if you are using 64 bit machine I think the commend sudo aptitude -y install ia32-libs libc6-dev-i386 lib32z1 is needed. Hope this can help you ~~
Have a great day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dan
Ok, I am trying to install ltib on Ubuntu 14.04, and I got other problem....
please, give me more "information", "How to", .... abut your gait
what is your Ubuntu ver ?
what is your ltib ver ?
from where I need to download the good ltib (my be I haven't the good libs ???!!!!)
Thanks
PF
Hi PF,
Which board are you using?
Best Regards
Dan
what I got on Ubuntu 14.04
ltib cannot be run because one or more of the host packages needed to run it
are either missing or out of date or not in ltib's standard path. Please
install/upgrade these packages on your host. If you have your own utilities
in non-standard paths, please add an entry into the .ltibrc file for example:
%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes
Package Minimum ver Installed info
------- ----------- ---------------
zlib 0 not installed
Died at ./ltib line 1397.
before this I do install zlib:
sudo apt-get install --reinstall zlib1g
and event more :
wget http://www.zlib.net/zlib-1.2.8.tar.gz
tar -xvzf zlib-1.2.8.tar.gz
cd zlib-1.2.8
./configure --prefix=/usr/local
make
sudo make install
Hi PF,
We have not test on the ubuntu 14.04. So I recommend you use ubuntu 10.04 or 12.04.For the BSP you can use L2.6.35_11_09_ER_SOURCE. You tell me you are using the chip IMX53-6AVV, I want to know which board are you using( the board designed by freescale or you design yourself), so I can give you right direction:smileyhappy:. Would you mind tell me ?
Best Regards
Dan
Hi Dan,
Nothing works, we have our own board based on IMX53.
This board is already working, and I haven't the old ltib, gcc etc.. so I need to
reinstall everything...
so please give me some "How to docs", How to use the patches....
thanks
PF
Hi PF,
I also want to know which reference design in freescale are you refer to ?
Best Regards
Dan
Hi PF,
Which version ubuntu are you using? You can refer to the doucment IMX53_1109_LINUXDOCS_BUNDLE. And here I attach a document for you.
Best Regards
Dan
Hi Dan
We are working on IMX53-6AVV
My computer is a Intel-CORE I7
For testing, I install VMware and I have Fedora 20, Ubuntu 14.04
Thanks
PF