Dear all,
We want to use PCIe on i.MX6.
The method of generate the Configuration Cycle is being known gradually.
Currently, the method of setting Data Link Layer to Active is investigated.
To this, I think that setting is required in an order from the physical layer.
Please recommend, if there are materials which are consulted.
And, which around in Source of Linux should be seen?
Best Regards,
George
Hi George, most suitable way to run SDK PCIe
example, please read included in package
iMX6_Firmware_Guide.pdf. Linux "L3.0.35_4.1.0_ER_SOURCE"
package can be found on the same link, in Linux package please read
i.MX_6Dual6Quad_Linux_Reference_Manual.pdf
"MX6_PLATFORM_SDK "
One can run tests from iRAM using scripts below
iRAM (OCRAM) i.MX6 SDK Application
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Chip,
I try to look for required information from the materials which you showed.
And it will post again here, when there is a question.
Thanks
Best Regards,
George