I'm Using Boundary Nitrogen6X Development board.
ENET connection is shown as below:
Physical <==> MII <==> MAC
KSZ9021RN is used in the design.
In the development board, RGMII_TD and RGMII_RD pins are connected to KSZ9021RN as data transfer pins.
BTW, ENET_RX_DATA & ENET_TX_DATA pins remains unused. What is the purpose of ENET_RX_DATA & ENET_TX_DATA in the ENET module?
Regards,
Anson
Solved! Go to Solution.
There are different pin sets for MII / RMII and RGMII. Please take a look at Table 23-1 (ENET External Signals)
of the i.MX6 DQ Reference Manual.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
There are different pin sets for MII / RMII and RGMII. Please take a look at Table 23-1 (ENET External Signals)
of the i.MX6 DQ Reference Manual.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yuri,
Does it mean ENET_RX_DATA & ENET_TX_DATA is used in MII or RMII mode, thus they are useless in RGMII mode?
e.g. we use MX6Q_PAD_ENET_RX_ER as SPDIF input :smileywink:
Yes, signals, that are not used for RGMII (say, ENET_RXD0), may be configured for other functionality.