AnsweredAssumed Answered

PF0100 SW1A/B output voltage

Question asked by MUTHU NAGARAJAN on Apr 21, 2014
Latest reply on May 7, 2014 by Jose Alberto Reyes Morales

Does the PF0100 SW1A/B output voltage of 1.375V during startup (F3 option for iMX6SoloLite) assume that the internal LDO_ARM in the iMX6SL is enabled? Follow on question, Once everything has powered-up, can I reduce the PF0100 SW1A/B output to 1.2V and bypass the internal LDO_ARM in the iMX6SL for normal operation? Same question for the PF0100 SW1C output for VDD_SOC_IN and VDD_PU_IN.

Outcomes