Hi,
I am trying to use the DAC using the micro controller MCF51MM256CLK with code warrior.
I've added the Init_DAC component from Peripheral Initialization.
Generating the processor expert code I obtained this error:
ERROR: Unexpected status of the scripts: Drivers\HCS08\Init_DAC_HCS08.rgi
I also noticed that in the list of supported item the MCF51MM256CLK is not listed, while I can find MCF51MM256_80/81/100/104. I don't know if the MCF51MM256CLK can be use anyway.
Could someone help me to fix this problem?
Thank you in advance!
Hello,
I could not reproduce the issue, I tried the Init_DAC component on the MCF51MM256CLK CPU with various settings and I never had any generation error. I used CodeWarrior 10.6.
Regarding the CPU, you can select the MCF51MM256CLK variant by adding a new CPU from the Component Library, Processors tab. A list with all available variants will be displayed. MCF51MM256CLK is the 80-pin variant.
Best Regards,
Cristian