AnsweredAssumed Answered

KL25Z bootloader, and Flash problem

Question asked by Amreen Sayyed on Apr 12, 2014
Latest reply on Apr 19, 2014 by Jorge_Gonzalez

Hello,

 

I m working with  freedom board KL25Z board.

I want to add boot loader and also I want a flash area to store configuration parameters specific to application.

 

I added "FLASH_LDD" component (from hardware component) of 1k size From the memory location 1FC00.

1. is it possible to protect this area from compiler to write unless otherwise I specify?

2. Also If I would like to define some parameters in this flash area at time of compilation, is it possible? how do I do that?

 

3. Also when I added "IntFLASH" component (from component library) for the boot loader,  I get the error for "FTFA" saying its already in use.

So is ii possible to use functions of "IntFLASH" component for the 1K flash where I an manually set the address of the memory location (instead in processor expert).

 

Regards,

Amreen

Outcomes