Looking for information on what needs to be done to modify the KINETIS_120MHZ_SC USBFS_device example for high speed USB (480Mb/s) operation using the TWR-SER2 board. Thanks.
Solved! Go to Solution.
Hi Peter,
Please check Kinetis USB Stack V4.1.1 from below link:
Customer can select K70 project and set "HIGH_SPEED_DEVICE" macro at <user_config.h> file.
#if (defined MCU_MK70F12) || (defined __MCF52277_H__)
#define HIGH_SPEED_DEVICE (1)
#else
#define HIGH_SPEED_DEVICE (0)
#endif
Wish it helps.
Best regards,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Peter,
Please check Kinetis USB Stack V4.1.1 from below link:
Customer can select K70 project and set "HIGH_SPEED_DEVICE" macro at <user_config.h> file.
#if (defined MCU_MK70F12) || (defined __MCF52277_H__)
#define HIGH_SPEED_DEVICE (1)
#else
#define HIGH_SPEED_DEVICE (0)
#endif
Wish it helps.
Best regards,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ma, I am trying to implement a vendor specific high speed device that implements a upstream (IN) speed test over a 512 byte bulk endpoint. The basis for this was copied from the CDC device example out of USB stack 4.1.1. The non control endpoints are are initialized with ZLT = 1:
(void)_usb_device_init_endpoint(&controller_ID, ep_struct->ep_num, ep_struct->size, ep_struct->direction, ep_struct->type, 1);
The device calls USB_Class_Send_Data() with 5*4096 bytes of data when the USB_APP_ENUM_COMPLETE event is detected, and then sends another 5*4096 byte block every time the
USB_APP_SEND_COMPLETE event occurs. This is working but it appears that the host also gets a zero length packet after each 5*4096 byte block. My question is how do I disable the zero length condition after each block I am trying to simulate a continuous stream. Thanks.
.