Please suggest exact method and best methodology which can used for flash programming of K60 chip .
the board has following interfaces : Ethernet , RS232,RS485
IDE; IAR WORKBENCH
controller : 100 pin
Debugger : OLIMEX-ARM-USB-OCD
the application we have as the ethernet & serial interfaces and we need to plan for the production . the image file to be used and excat method to be followed .
can we use ethernet boot loader or openocd can be used as standalone flash programmer .
thanks & regrds
vallinath
Hello vallinath:
We are sorry that you did not receive a response.
Did you clarify your doubt?
I cannot comment about the OLIMEX-ARM-USB-OCD tool, but since Kinetis parts are based on ARM cores, the available tools and programming solutions are many. It just depends on your needs.
Regarding bootloaders:
Ethernet: http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf
Serial: http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf
Regards!
Jorge Gonzalez
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers ) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.