AnsweredAssumed Answered

How to interface VGA display with imx6 Sabre Ai

Question asked by Ramakrishnan Venkatraman on Apr 6, 2014
Latest reply on Apr 7, 2014 by Ramakrishnan Venkatraman

Development Environment

 

Host - Windows 7, 64 bit

Board - imx6 Sabre AI

BSP - QNX SDP 6.6

Booting Type - SD Card

 

Things done so far

     1. I have downloaded QNX Neutrinos SDP 6.6 and installed in Windows 7, 64 Bit

     2. Using QNX Momentics to compile and got ifs-mx6x-sabreARD.raw file

     3. Formatted the SD card, Partioned the SD Card, Placed U-Boot and .raw file in the SD Card

     4. Used "HyperTerminal" in Windows host and connected to imx6 Board

     5. imx6 is booting with Qnx Neutrino and is displayed in the HyperTerminal

 

Things needed to do

     1. I have to interface a display with imx6 and should get an output on the display
     2. I am using HDMI for taking the video output

     3. I have connected HDMI to VGA converter and connected a VGA Monitor.  

 

Issue:

     I could not get any display in the VGA Monitor. What should I do to get a display in the VGA Monitor

 

Thanks in Advance..

 

Message was edited by: Ramakrishnan Venkatraman

Outcomes