i.MX6 HAB support in U-Boot 2013 and later

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 HAB support in U-Boot 2013 and later

1,174 Views
igorbezukh
Contributor I

Hi,

I would like to know whether HAB is supported in U-Boot 2013 or later versions?

Thanks and BR!

Igor Bezukh

0 Kudos
1 Reply

691 Views
igorpadykov
NXP Employee
NXP Employee

Hi Igor

yes supported, next Frescale linux kernel 3.10.17 Yocto release has U-boot 2013.4.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos