AnsweredAssumed Answered

i.MX6 trace connection

Question asked by vladislavkasik on Apr 4, 2014
Latest reply on Apr 4, 2014 by Yuri Muhin

Hi,

 

Is there any application note regarding the ARM trace connection on i.MX6 series for connecting DSTREAM or Lauterbach PowerTrace? None of the demo boards (SABRESDB, SABREAI) count with trace connection, they have only JTAG connector. Does the trace even work on i.MX6? According to the i.MX datasheet the trace signals are available as an alternate function on some pins and the frequency can be up to 600MHz so I assume that there must be some design recommendation.

 

Thanks,

Vladislav

 

Jiri Kotzian

Outcomes