When I connect my target to the terminal I can see the system features on Terminal monitor, consecuently it doesnt boot, i dont know why is this error, the serial port has all permissions, attached an image where the error can be seen, thaks!
Solved! Go to Solution.
Jacob, do you have a different terminal software to try it with?, like putty? Download PuTTY - a free SSH and telnet client for Windows
Are you using a Freescale board?, which OS are you loading?
It could be the terminal speed (check that it is 115200)
your terminal settings are 38400,8N1 but should be 115200,8N1