Hi
I have successfully run my Ethernet Driver on TWR-SER board for TWR-K70F120M but not working on TWR-SER2.
1. Is Ethernet Device in Single/Dual RMII mode is supported on TWR-SER2 board for TWR-K70F120M? According to this link, (Line: 241) it is not supported?
2. If supported, then is there any change in signal settings like (MDC, MDIO, CRS_DV, RXDn, RXErr, TXDn, TXEN and RMII_REF_CLK) as compared to TWR-SER board?
Regards
Seems you have created two threads for the same topic. Please kindly refer to Ethernet Device in Single/Dual RMII mode is supported on TWR-SER2 board for TWR-K70F120M for details.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. Kinetis Microcontrollers or MQX Software Solutions) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.