i.MX6 : Watchdog Timer Power-down counter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 : Watchdog Timer Power-down counter

1,517 Views
koichisakagami
Contributor II

Dear Sirs,


I am checking the i.MX6 Watchdog Timer module.

There is a Power-down counter in Watchdog Timer module.


The Power down counter with fixed timeout period of 16 seconds,
which if not disabled after reset will assert WDOG_B signal low.


This feature is intended to prevent the hanging up of core after reset,as WDOG is not enabled out of reset.

The WDOG_B signal is assigned at GPIO_9 [ALT1].
If the hanging up of core after reset is occurred,
the Pad Mux Register became default value by reset.
The WDOG_B signal function is not selected  at GPIO_9 pin.


I think that I can not watch the WDOG_B signal low at GPIO_9 by Power-down counter timeout.

Is my understanding correct ?

Or, by existing the special path for the Power-down counter timeout ,
can I watch the WDOG_B signal low ?


Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
2 Replies

535 Views
prabhatkumar
Contributor II

I would like use WDOG global signal for hardware watchdog. I have the same questions as above. Can someone please reply?

0 Kudos

535 Views
YixingKong
Senior Contributor IV

Koichi-san

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing