AnsweredAssumed Answered

Similar i.MX6Q NAND boot issues

Question asked by Anthony Czarnecki on Mar 28, 2014
Latest reply on Apr 15, 2014 by Yuri Muhin

I've been trying to get the i.MX6Q to boot from NAND on a custom board, but I've been having some trouble.

 

In this discussion, it looked like the a lot of information about the boot procedure was able to be read from the first 256 bytes of the boot log buffer.

 

Is there anyone that can interpret this or point me to where it might be documented?

 

S:0x000000D0:  0x00902190

S:0x00902190:    0x01    0x00    0x01    0x00    0xF0    0x00    0x02    0x00    0x00    0x00    0x03    0x00    0x01    0x00    0x04    0x00    0x00    0x00    0x0C    0x00    0x00    0x00   

S:0x009021A6:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021BC:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021D2:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021E8:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x009021FE:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902214:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x0090222A:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902240:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902256:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x0090226C:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

S:0x00902282:    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00    0x00   

Outcomes