AnsweredAssumed Answered

imx53qsb: STOP mode

Question asked by warl0rd on Mar 28, 2014
Latest reply on Jun 19, 2014 by warl0rd

Both  MCIMX53-START and MCIMX53-START-R board (aka imx53qsb, LOCO) boards run the Adeneo Android BSP 4.2. Is it possible to put those boards into the STOP mode as the Freescale Application note AN4270 mentions?? We are able to put the boards into the suspend mem mode and the total current consumption drops from 220 mA to 110mA (5V) which is still too much...

Outcomes