HI:
I am working on TWR-K53n512 with TWR-SER option. I have created the following test code by CW10.5 with MQX 4.0. The serial port works fine on the "ittyd" port. For my project, I need to use "ittye" port. In order to send and receive data with PC, I re-route the A41 and A42 pins on the TWR-K53n512 board to TWR-SER J17 and J19 pin 1. The same source code has been utilized with "ittye", the port doesn't work properly. I am able to set a break point before "write() function, and it looks like the port are receiving correct data. I have tried it on MQX 4.1 and got the same result. I wonder if anyone encounter any similar problem? Please let me know if you have any though. Thanks!
void Main_task(uint32_t initial_data)
{
void * fh_ptr;
int32_t param;
uint8_t serial_buffer[256];
uint8_t data_len;
printf("\n Serial Port ITTYE Test \n");
/* Initialize port */
fh_ptr = (void *)fopen("ittye:", (void *) (IO_SERIAL_RAW_IO | IO_SERIAL_NON_BLOCKING));
if (fh_ptr == NULL)
{
printf("cannot open file: ittye\n"); //print to uart0
}
param = 38400 ; //set communication baud
ioctl(fh_ptr, IO_IOCTL_SERIAL_SET_BAUD, ¶m);
param = 8;
ioctl(fh_ptr, IO_IOCTL_SERIAL_SET_DATA_BITS, ¶m); //set eight date bit
param = IO_SERIAL_STOP_BITS_1;
ioctl(fh_ptr, IO_IOCTL_SERIAL_SET_STOP_BITS, ¶m); //set one stop bit
param = IO_SERIAL_PARITY_NONE;
ioctl(fh_ptr, IO_IOCTL_SERIAL_SET_PARITY, ¶m); //set none parity bit
while (1)
{
data_len = read(fh_ptr,(void *)&serial_buffer,0xFFFF); //read() here is non-blocking function
if(data_len != 0)
{
write(fh_ptr,(void *)serial_buffer, data_len);
fflush(fh_ptr); //empty queue
_time_delay(1);
}
}
_mqx_exit(0);
}
The green color shows the data sent from PC to TWR-K53n512.
The yellow color shows the data sent from TWR-K53n512 back to PC.
Peter
Hi,
Please check using the user_config.h and twrk53n512.h files attached and let me know if this helps!!!
Have a great day,
Regards
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. MQX Software Solutions ) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.