AnsweredAssumed Answered

Shared Serial_LDD with MQX error message

Question asked by Adrian Rockall on Mar 25, 2014
Latest reply on Jun 11, 2014 by Petr_H

Hi,

 

I am just starting to use the stand alone Processor Expert Software 10.3. I have added the MQX component and now I want to add the Serial_LDD.

When I add it as Distinct Component everything is fine but if I add it as a Shared Component I get an error message telling me the Init method must be enabled when the MQX is selected. However the interface wont allow me to change the option to Generate Code for the component.

The Init method is set to generate code in the top level shared options.

 

Is this a bug or am I doing something wrong?

 

I have selected the MK60FX512LQ15 processor

 

Thanks,

Adrian.

Outcomes