performance monitoring of MPC5554

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

performance monitoring of MPC5554

672 Views
charlessaperste
Contributor II

we need to measure the processor utilization of out application using a MPC5554. are there any tools or sample code? thanks.

Labels (1)
0 Kudos
1 Reply

506 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hardware Performance Monitor module is available only on e200z7 cores. More info about the Performance Monitor can be found in:

http://www.freescale.com/files/32bit/doc/ref_manual/e200z760RM.pdf

If you have MPC5554 then only some software methods can be used: for example, if some kind of operating system is used, you can measure the time that application spends in idle task. Or you can measure the time needed for execution of some tasks (time base can be used – see application note AN2865 for SW example). Or whatever else – it depends what you need.

Regards,

Lukas

0 Kudos