About IBIS model of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IBIS model of i.MX6

Jump to solution
1,462 Views
okamotosatoshi
Contributor IV

Hello.

I want to check about i.MX6Q.

I want to check the configuration of the IBIS model of PCIe.

TX/RX is now setting the GPIO.

Is it correct what is to set the TX/RX?

(Voltage Level, Drive Storangth, Slew Rate etc...)

By the way , setting the CLK has become the LVDS.

Regards,

-okamoto

Postscript 2014/3/21

I am in a hurry to carry out the simulation.

I want you to provide information for carrying out the simulation.

//---------------------------------------------------------------------------

File Name : 21x21_imx6q_consmr_003.ibs

IBIS Version : 4.2

File Revision : 003

Date : Sun Mar 25 13:48:36 2012

//---------------------------------------------------------------------------

Is it corrected in the newest model?

Regards,

-okamoto

Labels (1)
Tags (3)
1 Solution
661 Views
Yuri
NXP Employee
NXP Employee

From section 9.5.6 (List of pins not modeled in the i.MX6 IBIS file) of “Hardware Development Guide

for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families …” : " ... some of the above unsupported pins are

described as “GPIO” cells. These are no more than placeholders and cannot be used for signal modeling"

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

View solution in original post

1 Reply
662 Views
Yuri
NXP Employee
NXP Employee

From section 9.5.6 (List of pins not modeled in the i.MX6 IBIS file) of “Hardware Development Guide

for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families …” : " ... some of the above unsupported pins are

described as “GPIO” cells. These are no more than placeholders and cannot be used for signal modeling"

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf