but this board tests fine when running the same test in room temperature.
we have modified some kernel code while doing this test:3. set the cpu freq in 1.2GHz and lock it.
we think if i.mx6q soc is really hot, it should reach the critical temperature(110℃) and reboot itself. this behavior seems not right.
any idea or suggestion would be appreciated. thanks.
reply from FAE, i.mx6Q using 1.2G must work in ldo_enable mode, can't force it work in ldo_bypass.