AnsweredAssumed Answered

where can i find gpu-viv-bin-mx6q.tar.gz  (version 4.6.8-1443)

Question asked by sky ocean on Mar 12, 2014
Latest reply on Jul 1, 2014 by Yixing Kong

hello everybody:

     now I am looking for gpu-viv-bin-mx6q.tar.gz(version 4.6.8-1443), as my kernel gpu driver is 4.6.8-1443.

     I have test:

     L3.0.15_12.02.00_SS_source/pkgs/gpu-viv-bin-mx6q-12.02.00(version 4.6.5)

     L3.0.15_12.05.02_SS_source/pkgs/gpu-viv-bin-mx6q-12.05.02(version 4.6.8)

     L3.0.35_3.0.0_source/pkgs/gpu-viv-bin-mx6q-3.0.0(version 4.6.9)

     L3.0.35_4.1.0_130816_source/pkgs/gpu-viv-bin-mx6q-3.0.35-4.1.0


I download the "L3.0.15" bsp from here:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_BSP_IMX


all of the libs will cause segment fault!

so , where can i down the right gpu-viv-bin-mx6q libs ?

Outcomes