AnsweredAssumed Answered

May I program *.bin image file into QSPI with DS-5

Question asked by Mehmet Ali Ipin on Mar 11, 2014
Latest reply on Mar 12, 2014 by Mehmet Ali Ipin

Dear Sir/Madam,

 

Hello,

 

We have VF3x prototype PCB, which we use dual QSPI Flash for boot. I developed and debugged our code with DS-5 debugger. Then I integrated the "bootloader_vybrid_qspixip" project source files into my project, built the *.axf file, then generated both *.bin and *.c image files. The *.c image file is about 5 times bigger then our *.bin file.

 

I read some documents mentioning that the IAR accepts *.bin file to program the QSPI flashes. But in DS-5 we only program big *.c files. I could not find a document about if it is possible to dwonload the *.bin files into the internal RAM and then program them to the QSPI flashes.

 

Could you please help me if it is possible within DS-5, or with MFGToolkit?

 

Thanks and best regards.

 

Mehmet Ali Ipin

Outcomes