AnsweredAssumed Answered

VPU firmware for i.MX6Solo.

Question asked by Satoshi Shimoda on Mar 5, 2014
Latest reply on Jun 23, 2014 by MaxTsai

Hi community,

 

I have some questions about i.MX6 VPU firmware.

In Linux BSP (L3.0.35_4.1.0), there are vpu firmwares in /lib/firmware.

Then, please see my questions below.

 

[Q1]

I want to know whether I can use vpu_fw_imx6q.bin for i.MX6Solo.

I think I can use it because i.MX6Solo has same VPU as i.MX6 Quad.

Is this correct?

Or there is a binary for i.MX6Solo?

 

[Q2]

If the answer for Q1 is "correct", i.MX6SDL and i.MX6DQ can use same binary file, isn't it?

However, there is vpu_fw_imx6d.bin in same directory.

What is this?

There is no description about this binary in i.MX_6Dual6Quad_VPU_API_Reference_Manual.pdf in Linux BSP documentation.

 

Best Regards,

Satoshi Shimoda

Outcomes