Hi , when i turn PE dev mode on, there is one line warning message in console as blow:
:{{DEVELOPMENT}} WARNING: Component GenericSWSPI was stored in the template in newer version: 01.018>01.001
and stopped in creating shared spi(0%) shown in status bar.
What reason can cause that problem ?
I'm using CW10.5 and PE 10.3.
Hi Kevin,
the reason is a bug in Processor Expert: it can get stuck while creating a shared component (I already have reported that problem).
To solve the problem, I have changed the setting of the component so the SPI bus is disabled at creation time (so you need to enable it after you have added the component).
Attached is the component with the workaround.
I hope this helps,
Erich