AnsweredAssumed Answered

iMx6 : VDD_HIGH_IN source

Question asked by Yannick Calmettes on Mar 4, 2014
Latest reply on Mar 5, 2014 by Yannick Calmettes

Dear All,

 

In most of iMx6 evaluation board VDD_HIGH_IN is supplied by a permanent source that is connected to VDD_SNVS_IN too.

When the PMIC PF0100 is switched off via PWRON input all the power sources are turned off and VDD_SNVS_IN is still powered but the problem is VDD_HIGH_IN is powered too.

Is the LDO that use VDD_HIGH_CAP is still ON ?

I did not see any sequence requirements on VDD_HIGH_IN, so is it possible to disconnect it from VDD_SNVS_IN and connect it to AUX_3V15 (SABRE board) ? of course VDD_SNVS_IN remains connected to the permanent source.

 

Best regards,

 

Yannick

Outcomes